Technical FAQs

Ask a Question

What is the definition of IP55 ?

The first ``5`` is for Dust protection and the second  ``5`` is for protection against water jets in all directions.


CTA-ID : 2008781
Was this helpful?
What can we do to improve the information ?