Technical FAQs

Ask a Question

Are Masterpact NW and NT circuit breakers 100% Rated?

Are Masterpact circuit breakers 100% Rated?

Product Line:
Masterpact NT and NW

NEMA influenced markets only

All UL 489 listed Masterpact NT and NW circuit breakers are 100% rated.
Note that standard 80% vs. 100% rating applies to breakers listed per UL 489 only.
Was this helpful?
What can we do to improve the information ?