Technical FAQs

Ask a Question

What are the coil voltage codes for the LC1D09 / LC2D09through LC1D38 / LC2D38 TeSys contactors?

Issue:
What are the coil voltage codes for the LC1D09 / LC2D09through LC1D38 / LC2D38 TeSys contactors?

Product Line:
IEC Contactors

Environment:
Ordering

Cause:
Selection

Resolution:
The following list the more common voltage suffix codes for these product lines.  For a more comprehensive list and to determine compatibility with a given product, refer to the catalog below.

AC Volts ___Code     AC Volts ___Code
12 ___ J7                   208 ___ LE7
21 ___ Z7                   220 ___ M7
24 ___ B7                  230 ___ P7
32 ___ C7                  240 ___ U7
36 ___ CC7               277 ___ W7
42 ___ D7                  380 ___ Q7
48 ___ E7                   400 ___ V7
60 ___ EE7                415 ___ N7
100 ___ K7                440 ___ R7
110 ___ F7                480 ___ T7
115 ___ FE7              575 ___ SC7
120 ___ G7                600 ___ X7
127 ___ FC7              690 ___ Y7
200 ___ L7                
               
Standard Coil                Low Consumption
DC Volts ___Code          DC Volts ___Code
12 ___ JD                           5 ___ AL
24 ___ BD                         12 ___ JL
36 ___ CD                         20 ___ ZL
48 ___ ED                         24 ___ BL
60 ___ ND                         48 ___ EL
72 ___ SD                         72 ___ SL
110 ___ FD                       96 ___ DL
125 ___ GD                     110 ___ FL
220 ___ MD                    220 ___ ML
250 ___ UD                     250 ___ UL
440 ___ RD                



CTA-ID : 2011595
Was this helpful?
What can we do to improve the information ?