Technical FAQs

Ask a Question

What are the coil voltage codes for the LC1D115 / LC2D115 and LC1D150 / LC2D150 TeSys contactor?

Product Line:
 
Tesys D line Contactors
 
Resolution:
 
The following list the more common voltage suffix codes for these product lines.  For a more comprehensive list and to determine compatibility with a given product, refer to the catalog below.

Note 1: LC1D150 contactors are only available with *7 coil codes.
Note 2: Coil Code ending number represents frequency rating as follows:
5 = 50 Hertz
6 = 60 Hertz
7 = 50/60 Hertz

AC Volts ___Code                DC Volts ___Code
24 ___ B5 or B6 or B7        12 ___ Not Avail.        
42 ___ D5 or D7                24 ___ BD
48 ___ E5 or E6 or E7        36 ___ CD
110 ___ F5 or F6 or F7        48 ___ ED
115 ___ FE5 or FE7                60 ___ ND
120 ___ G6 or G7                72 ___ SD
127 ___ FC5 or FC7                110 ___ FD
208 ___ L6 or LE7                125 ___ GD
220 ___ M5 or M6 or M7        220 ___ MD
230 ___ P5 or P7                250 ___ UD
240 ___ U5 or U6 or U7        440 ___ RD
277 ___ W6 or UE7                
380 ___ Q5 or Q6 or Q7                
400 ___ V5 or V7                
415 ___ N5 or N7                
440 ___ R5 or R6 or R7                
480 ___ T6 or T7                
500 ___ S5 or S7                



CTA-ID : 2011967
Was this helpful?
What can we do to improve the information ?