Technical FAQs

Ask a Question

What is the difference between Type 1 & Type 2 coordination?

Issue:
What is  the difference between Type 1 & Type 2 coordination?

Product Line:
Starters and Contactors

Environment:
Definition

Cause:
Clarifying

Resolution:
Type I - Under short circuit conditions, the contactor or starter shall cause no danger to persons or installation and may not be suitable for further service without repair and replacement parts.

Type II - Under short circuit conditions, the contactor or starter shall cause no danger to persons or installation and shall be suitable for further use. The risk of contact welding is recognized, in which case the manufacturer shall indicate the measures to be taken in regards to equipment maintenance.

For additional information on Understanding Type 2 Coordination please refer to Link below.

http://static.schneider-electric.us/docs/Motor%20Control/0140PD9202A.pdf
 
Was this helpful?
What can we do to improve the information ?