Technical FAQs

Ask a Question

What is the altitude derating for a TeSys D-Line contactor?

Product Line:
 
Tesys D line Contactors

Resolution:
 
The contactors are fully rated up to 3000 meters. Following are derating multipliers for altitudes above 3000 meters for both voltage and current:

Voltage
3500m x 0.90
4000m x 0.80
4500m x 0.70
5000m x 0.60

Current
3500m x 0.92
4000m x 0.90
4500m x 0.88
5000m x 0.86

For example, an LC1D80 at 5000 meters:
- The maximum rated operational voltage is 1,000V (IEC947-4) and 690V (UL/CSA). At 5000 meters it becomes 1000V x 0.6 = 600V (IEC947-4) and 690V x 0.6 = 414V (UL/CSA).
- The maximum rated operational AC3 current is 80A. At 5000 meters it becomes 80A x 0.86 = 68A.



CTA-ID : 2015524
Was this helpful?
What can we do to improve the information ?