Technical FAQs

Ask a Question

What, if any, are the mounting restrictions for the U-Line starter operating positions ?

The devices are limited to a tilt (front to back ) of no more than 30 degrees from vertical and a sway (sideways) of no more than 90 degrees to the left or the right.


CTA-ID : 2016187
Was this helpful?
What can we do to improve the information ?