Technical FAQs

Ask a Question

With the ATV58, ATV61, or ATV71 analog output set for output frequency, why does it only provide 17ma when the drive output frequency is 60hz?

The analog output provides a signal proportional to the motor frequency estimated by the drive controller.
The minimum configured value corresponds to zero.
The maximum configured value of the analog output corresponds to the maximum frequency setting (tFr), not the high speed setting (HSP).
The default tFr setting is 20% higher than the HSP. (72 hz for 60 hz applications, 60 hz for 50 hz applications)
Need to set the tFr parameter to 60 hz to match the HSP setting of 60 Hz.
Lowering the maximum frequency setting may result in nuisance Overspeed faults.


CTA-ID : 2016918
Was this helpful?
What can we do to improve the information ?