Technical FAQs

Ask a Question

Is a LC1D40 thru LC1D150 available with a low consumption DC coil?

Issue: 
Are the larger amperage d line contactors available with low consumptions coils? 

Product Line:
 Tesys D line contactors

Environment:
Products sold and used in the United States
 
Cause:
 Identifying available product lines
 
Resolution:
 
No. Low consumption coils are available only on LC1D09 thru D38 contactors.



CTA-ID : 2020741
Was this helpful?
What can we do to improve the information ?