Technical FAQs

Ask a Question

Can the 0-10VDC analog input be configured for 0-5VDC on the Altivar 71 drive?

Yes, There are scaling parameters for AI1 in menu 1.5 that allow you to change the min and max values of the speed reference (UIL1 and UIH1 for AI1).  Once these parameters are set, the speed referrrence is linearly scaled between them.

CTA-ID : 2025179
Was this helpful?
What can we do to improve the information ?