Technical FAQs

Ask a Question

Which ATV71 drives have the built in braking transistor?

Models with a rating of 160KW (250HP) or less have a built-in braking transistor.
ATV71H...M3, ATV71H...M3X and ATV71H075N4 to HC16N4 drives have a built-in dynamic brake transistor.
For ATV71HC20N4 to HC50N4 drives, a separate braking unit must be used.


CTA-ID : 2026409
Was this helpful?
What can we do to improve the information ?