Technical FAQs

Ask a Question

How to get system clock time during runtime to be displayed on Vijeo Citect screen.

In Vijeo Citect, to get system clock time parameters use of Cicode script has to be done using Cicode Time Functions, as there are no pre-defined system tags available.

Example for reading ‘Second’ parameter of system clock in Vijeo Citect.

FUNCTION Time_Read()
INT sec_var;
Similarly Cicode script can be written for reading Minute & Hour parameters of system clock.

Was this helpful?
What can we do to improve the information ?