Technical FAQs

Ask a Question

Where is the thermal overload reset button located on the U-Line starter?<br /><br />

The reset handle is located on the power base and moves to the tripped position upon sensing a short circuit or overload fault.

CTA-ID : 2027486
Was this helpful?
What can we do to improve the information ?