Technical FAQs

Ask a Question

What is the difference between a Zelio Plug-In relay socket with "mixed" vs. "separate" contact terminals ?

Issue:
What is the difference between a Zelio Plug-In relay socket with "mixed" vs. "separate" contact terminals ?

Product Line:
Relays and Timers

Environment:
All products

Cause:
Product Features

Resolution:
Sockets with "mixed" terminals have input terminals mixed together on the same side with coil terminals and are one or 2 tier design . Sockets with "separate" terminals have inputs and outputs on the same side in 2 or 3 tiers while the coil terminals are on the opposite side .


CTA-ID : 2030914
Was this helpful?
What can we do to improve the information ?