Technical FAQs

Ask a Question

How to establish Magelis XBT GT communication with M340 PLC using USB cable.

In order to establish communication of XBT GT Magelis Terminal using standard USB Cable with M340 PLC you have to set the PLC IP to 90.0.0.1 for Modbus TCPIP driver in Vijeo Designer. 

Was this helpful?
What can we do to improve the information ?