Technical FAQs

Ask a Question

How to connect the Altistart 48 to motor delta terminal with existing star delta starter as bypass arrangement.

The Circuit diagram of Altistart 48 connection to motor delta terminals with existing star-delta starter as bypass arrangement is attached.
Was this helpful?
What can we do to improve the information ?