Technical FAQs

Ask a Question

What is the explanation of the Parameter FLC1 in TeSys T.

FLC1 is the parameter to enter the Motor nominal current in TeSys T. In this parameter, the Motor nominal current is entered as a percentage of the rated value of the TeSys T. 

Example:
 
For TeSys T of range 8Amps (LTMR08) and a motor of 2 Amps nominal current, you have to set the FLC1 value to 25% because the Motor nominal current is 25% of the full load current of TeSys T Module (LTMR08).
 
This means that the current in register 466 (value of current in percent) take the value of 100% when you reach 25% of the current of the TeSys T Module rated current value.
Was this helpful?
What can we do to improve the information ?