Technical FAQs

Ask a Question

What are the Auxiliaries that can be used with C60H-DC.

Refer the attached documents for the list of Auxiliaries that can be used with C60H-DC.

1. For the list of Auxiliaries that can be used with C60H-DC as per IEC certification refer attachment 90081.pdf
 
2. For the list of Auxiliaries that can be used with C60H-DC as per UL certification refer attachment 91103.pdf
Was this helpful?
What can we do to improve the information ?