Technical FAQs

Ask a Question

How to convert a Modsoft Program to a Concept database.

The procedure for converting the ModSoft program into a Concept

Database is as follows:
1 Open the Modsoft Converter from the Concept utility. (Start menu, Concept, Modsoft Converter).
2 Go to the file converter and select the Modsoft file (.env extension) that you wish to convert.
3 Click OK and this will automatically create a .prj file that can be run with Concept. 
Was this helpful?
What can we do to improve the information ?