Technical FAQs

Ask a Question

What are the different part references for the programming software and communication cable to be used for Modicon Micro Range PLCs.

There are three different PL7 software packages that can be used for programming of the Modicon Micro Range of PLCs. 

1. TLXCDPL7PP45M.....PL7 PRO Software package.
2. TLXCDPL7MP45M.....PL7 Micro Software package.
3. TLXCDPL7JP45M.....PL7 JR Software package.
                           
The programming cable must be ordered separately. There are two options for the cable:
 
1. For Serial:
 
a. TSXPCX1031.....Multi-Function Serial Communication Cable.
 
2. For USB:
 
a. TSXCUSB485.....USB to RS485 Serial Converter.
b. TSXCRJMD25.....9 pin Serial to 8 pin mini DIN cable.
Was this helpful?
What can we do to improve the information ?