Technical FAQs

Ask a Question

What is the internal wiring connection of Motor Mechanism Module (MT100 to MT630) for Compact NS <630 MCCB range.

Refer the attachment for the internal wiring connection of Motor Mechanism Module (MT100 to MT630) for Compact NS < 630 Moulded Case Circuit Breaker (MCCB).

Was this helpful?
What can we do to improve the information ?