Technical FAQs

Ask a Question

How many devices/registers can be IO scanned by 140CPU65160 Module, Modicon Quantum Range.

140CPU65160 can IO scan up to 128 devices/registers maximum.

The total number of input and output words which can be scanned during one cycle is 4000 each.
The maximum number of devices which can be used for IO scanning differs according to the type of module.
Below table shows the IO scan limitation for Modicon Quantum range CPUs.
Was this helpful?
What can we do to improve the information ?