Technical FAQs

Ask a Question

What is the minimum rating of the Motor that can be used with the Altivar 31/61/71 Range of Drives.

The motor current should not be less than 0.2 times the nominal Drive current when the motor is driven by Altivar 31/61/71 Drives, for thermal protection.

However, the programming of the parameters should be as per the motor nameplate data for safety of the motor.
Was this helpful?
What can we do to improve the information ?