Technical FAQs

Ask a Question

What is the minimum time interval allowed between two consecutive peaks of 220% Torque (Tn) in Altivar 71 Drive.

The Altivar 71 Drive can deliver the peak Torque (Tn) of 220% consecutively within a minimum time interval of 5 minutes.

Was this helpful?
What can we do to improve the information ?