Technical FAQs

Ask a Question

Which are the environmental conditions in which the Hoist Resistor of Altivar 71 Drive be used.

The environmental conditions applicable for the Altivar 71 Drive Hoisting Resistor usage are: 

1. Relative Humidity range from 5% to 93%, without condensation or dripping.
2. Air must be without corrosive gas, dust and condensation.
Was this helpful?
What can we do to improve the information ?