Technical FAQs

Ask a Question

Is the remote keypad option available for Altivar 21 Drive.

Yes, the remote keypad option is available for the Altivar 21 Drive. The reference for the same is VW3A21101. It can be installed remotely up to a distance of 5 meters maximum.

Refer to attached document for the kit part reference, Kit contents and Functional Instructions.
Was this helpful?
What can we do to improve the information ?