Technical FAQs

Ask a Question

What is the Boot-up Time of Altivar61/71 Drives on Power Up.

The Boot-up Time of Altivar61/71 on Power Up (switch-off/switch-on) is approximately 2 seconds. 

During this time, following processes take place inside the drive:
1. Charging of the capacitors.
2. Initialization of the internal switch mode power supply.
3. Initialization of the microprocessor
4. Reading of the EEPROM.
5. Synchronization of the microprocessors.
Was this helpful?
What can we do to improve the information ?