Technical FAQs

Ask a Question

What is the minimum Power suite software version required for Bluetooth Adapter on Altivar 31.

The minimum Power Suite version for using the Bluetooth feature with Altivar 31 Drive is V2.2.

The part reference for the Bluetooth adapter is VW3A8114. 

The maximum communication distance allowed is 10 meters.
Was this helpful?
What can we do to improve the information ?