Technical FAQs

Ask a Question

What is the Line dip Ride Through time for the Altivar 71 and Altivar 61 Drives.

Maximum running time (without fault) at Under Voltage with Nominal Torque is: 

1. 1000 msec. with a voltage 70% of nominal voltage (UrEs).
 
2. 500msec. with a voltage 40% of nominal voltage (UrEs).
Was this helpful?
What can we do to improve the information ?