Technical FAQs

Ask a Question

What is the maximum cable length allowed between PC and TeSys T for connection via PowerSuite.

The maximum cable length allowed between PC and TeSys T connection via PowerSuite depends on the system and the converter used.

If the standard converter, from PCP offer which comes with VW3A8106 Kit, is used then the maximum recommended cable length is 10 meters.

In case of using a RS 232/485 converter with an external power supply, the maximum cable length can be 1000 meters.
Was this helpful?
What can we do to improve the information ?