Technical FAQs

Ask a Question

What is the Short Circuit rating of LU2B starters in TeSys U as per UL508 TypeE specification?

The Short Circuit rating of LU2B starters in TeSys U as per UL508 TypeE specification is as follows: 

 
Voltage (V AC) Short Circuit Rating (KA)
440 50
500 10
690 4
 
The breaking capacity can be increased by using the limiters like LA9LB920 with TeSys U power base. Refer to the attached.
 
 
 

 

Was this helpful?
What can we do to improve the information ?