Technical FAQs

Ask a Question

What is the maximum current which can be measured by TeSys T.

810 A is the maximum current that can be measured by the TeSys T as per the Schneider Electric offer catalogue.

However, as per the TeSys T hardware/software design you can go up to 1000 Amps. using external CT (not in the Schneider Electric offer).

Was this helpful?
What can we do to improve the information ?