Technical FAQs

Ask a Question

Do the Energy and Power values remain stored in Micrologic P during Power Outage.

The Energy and Power values remain stored in Micrologic P even when the Power Supply is not available as all the values get stored in the EEPROM memory.

 

EEPROM is nonvolatile memory and can store values for a very long time without battery backup.

Was this helpful?
What can we do to improve the information ?