Technical FAQs

Ask a Question

How many Mechanical Operations can be done with Evolis Circuit Breaker.

Evolis Circuit breaker comply the Class M2 of IEC 62261-100 Standards.


As per class M2 of IEC Standard, the circuit breaker can be operated up to 10000 Mechanical Operations.

Was this helpful?
What can we do to improve the information ?