Technical FAQs

Ask a Question

What is the maximum length of the connector cable between the LTMR and LTME module in TeSys T Range.

Three different length connectors are available for connecting the LTMR and LTME module.

The maximum length between the connections of TeSys T controller (LTMR) and Expansion Module (LTME) module is 1 meter.

Was this helpful?
What can we do to improve the information ?