Technical FAQs

Ask a Question

Are the Multi 9 circuit breakers and supplementary protectors considered ``trip free``?

``Trip Free`` means the breaker will trip in an overcurrent situation even if the handle is locked in the ``on`` position. These breakers are considered trip free.

CTA-ID : 2051946
Was this helpful?
What can we do to improve the information ?