Technical FAQs

Ask a Question

What does sealed VA mean?

The sealed VA is the current draw when the coil is energized after the contacts have closed. This is the stable condition which uses the least
current, as opposed to inrush VA, where changing contact state requires high current for a brief period.


CTA-ID : 2051975
Was this helpful?
What can we do to improve the information ?