Technical FAQs

Ask a Question

Can an F-Line contactor be backfed?

Yes. Electrically, the F Line contactor can be backfed. However, a UL inspector may have an objection, because of the L1 L2 and L3 line side marking and the T1 T2 and T3 markings on the load side.

CTA-ID : 2051960
Was this helpful?
What can we do to improve the information ?