Technical FAQs

Ask a Question

What is the difference between a LULC031 Modbus communication module and a LULC033 Modbus communication module.

The LULC031 does not provide and extra input and there are no fault registers for communication failure, both a prevelant with the new LULC033 module

CTA-ID : 2053932
Was this helpful?
What can we do to improve the information ?