Technical FAQs

Ask a Question

What size cable does a LAD7B10 accept?

Need to know the size cable accepted by the LAD7B10 block

Product Line:
IEC Contactors and starters

Products sold and used in the United States

Identifying cabling requirements

It takes either a 1 flexible cable without cable end size 14-8 AWG or 1 flex cable with cable end size 16-12AWG or 1 solid cable without cable end size 16-10 AWG

CTA-ID : 2053970
Was this helpful?
What can we do to improve the information ?