Technical FAQs

Ask a Question

What type of connections are available from ABE9 base to connecting PLC / Control system?

The ABE9 product range has two different types of connection back to the control system :-

1) Pre made Multi core cable via cable gland (IP67) choice of two lengths of flying lead 5 and 10 M

2) M23 19 pin plug connector
Was this helpful?
What can we do to improve the information ?