Technical FAQs

Ask a Question

What size screen and resolution are available for the iDisplay product range?

There are two sizes available 15" VGA (1024 x 768) and 19" SXGA (1280 x 1024).
Was this helpful?
What can we do to improve the information ?