Technical FAQs

Ask a Question

What is the default IP address of the TSXETZ Ethernet gateways?

The default Ethernet interface IP address for the TSX ETZ module is derived from it’s MAC address which is printed on the ETZ module:

085.016 is common to 'all' ETZ modules. where xxx and yyy are the last two numbers of the MAC address.


The module’s MAC address is (in hexadecimal): 00 80 F4 01 12 20
In this case the default IP address is (in decimal):
Was this helpful?
What can we do to improve the information ?