Technical FAQs

Ask a Question

What are the differences in the TSXETG1000 series product we offer?

The TSXETG1000 is an Ethernet (Modbus TCP / IP) to Modbus RTU gateway.
The TSXETG1010 is an Ethernet (Modbus TCP / IP, or XWAY TCP/  IP) to Unitelway gateway. So is only likely to be used with TSX37 Micro and TSXP57 Premium product ranges.

Both modules are free standing, and come with WEb Designer software which is used to configure them. Customer web pages can be added using Microsoft front page.
These modules support Ethernet II and Ethernet 802.3 framing. Both modules are classed as  C20 / C30 configurable web servers.

For more detailed summary of features see attachment.
Was this helpful?
What can we do to improve the information ?