Technical FAQs

Ask a Question

What is the IP rating of RM6

RM6 has an IP rating of IP3X on the front face and the gas tank is rated at IP67.

For more information on RM6 please click here or e-mail:
Was this helpful?
What can we do to improve the information ?