Technical FAQs

Ask a Question

What operating systems are available on the Magelis Smart Industrial PCs?

The Operating System on the Magelis Smart and Smart+ is Windows XP Embedded
The operating system is embedded in the device as the Magelis Smart and Smart+ have no hard disk

The full details of the software included is listed below
  • Windows XP with language support for English, French, Spanish, Italian, German, Swedish, Chinese, Russian and Portuguese
  • framework.NET Run Time
  • Web Application
  • Vijeo Designer Run Time Trial version (21 days)

in addition for the 15" Models
  • Vijeo Citect Web Client
  • Office Reader
Was this helpful?
What can we do to improve the information ?