Technical FAQs

Ask a Question

What is the definition of a power transformer

The definition of a power transformer as stated in IEC 60076 Part 1 is as follows :-

A static piece of apparatus with two or more windings which, by electromagnetic induction, transforms a system of alternating voltage and current into another system of voltage and current usually of different values and at the same frequency for the purpose of transmitting electrical power
Was this helpful?
What can we do to improve the information ?