Technical FAQs

Ask a Question

What is the definition of a transformer on-load tap-changer

A device for changing the tapping connections of a winding, suitable for operation while the transformer is energized or on load
 
NOTE The values are related to the principal tapping, unless another tapping is specifically stated.
Was this helpful?
What can we do to improve the information ?