Technical FAQs

Ask a Question

Which networks are supported on the Modicon Momentum by Communication adapters

The following networks are supported by Modicon Momentum Communication adapters

Communication adapters for Ethernet TCP/IP
170 ENT 110 02 Transparent Ready Class A10
170 ENT 110 01 Transparent Ready Class B20
 
INTERBUS SUPI 3
170 INT 110 03 Twisted Pair
170 INT 120 00 Fibre optic
 
INTERBUS I/O bus SUPI 2
170 INT 110 00 Twisted Pair
 
Profi bus DP
170 DNT 110 00
DeviceNet
170 LNT 710 00
 
Modbus Plus
170 PNT 110 20
170 PNT 160 20
170 NEF 110 21
170 NEF 160 21
 
Fipio
170 FNT 110 00
170 FNT 110 01
Was this helpful?
What can we do to improve the information ?