Technical FAQs

Ask a Question

Is it possible to connect Altivar 312 and Altivar 71 drive on the same DC bus.

 

The Altivar 312 and Altivar 71 cannot be connected on the same DC bus.
The Over Braking Fault (OBF ) threshold of ATV312 is 880V and the OBF of ATV71 is 825V .That make incompatible both the products connected in same DC bus.
Was this helpful?
What can we do to improve the information ?